I am having trouble getting any connected keyboard to use a standard US English command. If I type “-” I get “+”. The only close option in Setup is Int’l English and that does not work.
This language option in setup will only change the onscreen language, not the keyboard input language. You’ll need to change this within Linux, I don’t have a real robot infront of me to check but I think you need to change the XKBLAYOUT line to =“us” in /etc/default/keyboard and then reboot.
Hi @ajp
conecting this thread Keyboard setting
I have the same problem, looked into your solution with our IT guy, but we don’t see a way to change the keyboard input language.
can you eleborate more about your solution?
would have tought to find it here:
thanks in advance,
Corné
Hi @anon32310726,
You need to do the following steps
- Go to the terminal by pressing CTRL+ALT+F6
- type in “root” as user and admin password default is “easybot”
- type in “nano /etc/default/keyboard” and hit enter
- modify the file according to @ajp instruction
- press CTRL+X to exit and save changes
- reboot the system
I hope that solves your challenge
Ebbe
I can’t get the password for URSim to work.
ursim login: root
password: easybot
Login incorrect
Please consider that your keyboard layout can affect the password you type in
Not trying to be rude but that doesn’t really help.
I did test this, though… I typed the user name as easybot and it came out correctly. When I type in root as the username it came out correctly.
Hi @anon32310726 ,
You could refer to this article to solve your problem.
Hi @anon507564 ,
In the URsim, the default keyboard setting is US already so why do you need a password? Do you want to change it to other keyboard layout?
If you really need to log in the ubuntu as “root” with a new password in ursim, you could follow steps below in the terminal console. I suggest you still use “easybot” as the password to avoid forgetting it.

I was actually trying to use it to use the file manager. Figured it was the same.
Not a biggie. I can use shared folders. Takes longer to set up but works fine.
URSim is set up using user “ur” where as the real robot just uses root. I would guess that’s why it was telling you the password was wrong in URSim… easybot is the password for ur not root?