Im using the UR10e with UR_RTDE and i am controlling the robot in ForceMode. Now the thing that i want to do is, that the robot should be controlled in ForceMode on the z-Axis to hold the contact with a subject with for example 10 N, and at the same time i want to control the robot on the x- and y-Axis via speedL.
So my question now is, if it is possible to do this or is there any other solution to control the robot speeds while being in ForceMode?