Hello All
has anyone ever communicated remote I/O Turkc with universal robots only controller and I/O.
can you tell me if this is possible and if there is literature?
thanks.
Hello All
has anyone ever communicated remote I/O Turkc with universal robots only controller and I/O.
can you tell me if this is possible and if there is literature?
thanks.
You should be able to connect a Turck I/O block (Modbus) to the UR via an ethernet connection.
See User Manual section 24.20. MODBUS Client I/O Setup
https://www.universal-robots.com/download/?filters[]=98757&query=
Yes, we use the TBEN series of remote IO blocks with modbus directly on the robot, they work really well for us.
We use the TBEN-L5-16DXP modules as I like they are sealed, and each of the 16 points is configurable as an input or output. Ultimate flexibility.