Check if Modbus or Profinet are activated

through the API you can only read the Standard Digital I/O so actually there is no proper solution for that yet. If you don’t need real time response you can do the following:

  1. create a global variable
  2. send a program to the robot through secondary client which modifies your variable with a line e.g. var1 = read_input_boolean_register(0) with URCap Sample: Send Script with button push URCap
    also note that you need to modify it to send multiple lines of urscript code: Secondary Client Issue
  3. read your variable through the API