Check and link variables continuously

Hello,

I need to check a Variable for 5 Sec. so that the Sensor is not activated by mistake.

the Programm should only run if the Sensor gets the Signal for that time.

Should i use a Sub-Programm?

Kurt.stahl,

You could monitor the input in a thread.
when the input goes high start a timer
when the input goes low stop and reset the timer
remember to add a sync() into the thread
then in your program
check if the input is high and timer to be equal or grater than 5 sec.

so if the input is activated for less than 5 sec the if statement in the prog won’t be true because the timer will keep being reset to 0
if the input is activated for 5 sec or more the timer will start continue to count until the Digital input is low again. (or you stop the timer somewhere else in the program).

image

Another simple way to achieve this is to use an if-command with the continuously checking of the expression in a thread such as this: