I downloaded the urcap sdk-1.10.0.
There are no permissions of files unzipped on linux.
But it’s no problem to copy unzipped files to linux after these are unzipped on windows 10.
Hi,
the files are broken. I have the same issue. @inu can u help us again ? 
Hi @fujikit and @m.birkholz,
I think you should be able to fix it with the chmod.
I have uploaded a new zip file. So downloading a new zip file is also an option.
To @Ebbe
Thank you for your fixing the issue.
I verified that the unzipped files had no problem.