Greetings URCommunity,
In my application, I have two identical encoders. One of them is connected to the robot, the other to a camera. I would like to know if it is possible to synchronize them. For instance, the one connected to the robot has a different tick count than the one of the camera and I would like them to be the same. I can’t change the value of the camera one, so I was hoping I could switch the one of the robot
For example,
The encoder connected to the camera has a current tick count of 1000 and the robot has 3000. I want them to be always equal
Is it possible to synchronize them?
Best regards,
Pedro Monforte