Hi Forum,
I am trying to catch a High Signal through the Tool Digital Input port(the one on the flange) using secondary client interfaces in real time. I was able to catch the signal changes under Digital input
bits. When I give an input high, we receive 40F0 0000 0000 0000 0000.
however, I don’t know what each bit corresponds to. For example, in the manual, it says that there are 8 bytes for the digital inputs, but we have 8 configurable inputs, 8 general inputs, and 2 Tool Inputs. Now, what are the ranges for the Tool Inputs?
Anything that is related to this question can be helpful!
Thanks,
Richard