Download URCaps SDK

PolyScope 3.5.0.10584 has been released November 27th 2017.

URCaps SDK v. 1.2.41
SKYFISH DOWNLOAD

FTP download:
Host: ftp.universal-robots.com
User: URPlus
Pass: 2q6C36ZZ

Release notes for software version 3.5.0.10584
Release notes

This is a major release of the SDK, raising from 1.1 to 1.2.
There are many new features to the new SDK, including:

  • Support for configurations of “built-in” PolyScope program nodes
  • Support for getting a robot position defined by the user through the ‘Move’ tab
  • Support for accessing, creating and storing variables
  • Support for capturing click/touch pixel positions in GUI elements
  • Support for getting the selected language, programming language and unit type settings

Please refer to the updated URCaps tutorial and the release notes for PolyScope 3.5.0.10584.

1 Like