URCaps SDK v. 1.0.0.7 (released May 31st 2016)
Download
Released along with PolyScope 3.3.0.145.
Release notes.
PolyScope 3.3.1.237 has been released August 1st 2016.
URCaps and SDK is not affected.
Release notes.
PolyScope 3.3.2.266 has been released September 8th 2016.
URCaps SDK v. 1.0.0.23
Download
Release notes for Software version 3.3.2.266
Release notes
There are no release notes relevant to URCaps SDK.
PolyScope 3.3.3.292 has been released October 25th 2016.
URCaps and SDK is not affected.
Release notes
PolyScope 3.3.4.310 has been released December 16th 2016.
URCaps SDK v. 1.0.1-8
Download
Release notes for Software version 3.3.4.310
Release notes
The change relevant to URCaps SDK is a fix regarding the install.sh script, that asks whether the UR Tool chain should be installed. This can only install in 64-bit Linux, preferably with Intel chip.
If you have already installed the SDK succesfully, no actions are needed.
PolyScope 3.4.0.39 has been released March 14th 2017.
URCaps SDK v. 1.1.0.76
SKYFISH DOWNLOAD
FTP download:
Host: ftp.universal-robots.com
User: URPlus
Pass: 2q6C36ZZ
Release notes for software version 3.4.0.39
Release notes
This is a major release of the SDK, raising from 1.0 to 1.1
There are many new features to the new SDK, including:
-
Ability to add your own URScript functions to the Functions list in the Expression Editor.
New sample enclosed in the SDK to demonstrate this feature. -
Ability to create sub-trees for program nodes, i.e. for generating templates.
New sample enclosed in the SDK to demonstrate this feature. - Ability to choose which API version to use, when developing a URCap.
- Automatic annotation for contributed script code for improved debugging.
- Improved feedback for programs missing a URCap used in the program
- Improved URScript debugging functionality
- New keyboard editor.
Please refer to the updated URCaps tutorial and the release notes for PolyScope 3.4.0.39.
PolyScope 3.5.0.10584 has been released November 27th 2017.
URCaps SDK v. 1.2.41
SKYFISH DOWNLOAD
FTP download:
Host: ftp.universal-robots.com
User: URPlus
Pass: 2q6C36ZZ
Release notes for software version 3.5.0.10584
Release notes
This is a major release of the SDK, raising from 1.1 to 1.2.
There are many new features to the new SDK, including:
- Support for configurations of “built-in” PolyScope program nodes
- Support for getting a robot position defined by the user through the ‘Move’ tab
- Support for accessing, creating and storing variables
- Support for capturing click/touch pixel positions in GUI elements
- Support for getting the selected language, programming language and unit type settings
Please refer to the updated URCaps tutorial and the release notes for PolyScope 3.5.0.10584.