# URSim issues: Robotiq Grippers Installed but not Working

**URL:** https://forum.universal-robots.com/t/ursim-issues-robotiq-grippers-installed-but-not-working/15692
**Category:** Technical Questions
**Created:** [July 30, 2021, 5:52pm UTC](https://forum.universal-robots.com/t/ursim-issues-robotiq-grippers-installed-but-not-working/15692 "2021-07-30T17:52:45Z")
**Posts on this page:** 7
**Page:** 1

<div class="post-metadata">

### Author: ![anon507564](https://avatars.discourse-cdn.com/v4/letter/a/e480ec/32.png) [@anon507564](https://forum.universal-robots.com/u/anon507564)
#### Post date: [July 30, 2021, 5:52pm UTC](https://forum.universal-robots.com/t/ursim-issues-robotiq-grippers-installed-but-not-working/15692/1 "2021-07-30T17:52:45Z")

</div>

I’m trying to do more initial programming in the office instead of on the floor. I installed URSim a while back and am trying to get it to run my programs from the floor.

Robotiq Grippre URCaps version 1.8.7.10599 is installed and active in URSim.  
PolyScope version 5.10.0.106288 is installed and running in URsim.

The grippers don’t show up on the Installation/URCaps/Grippers dashboard and they don’t register in the program. When the program gets to those nodes it says Gripper 1 (or 2) must be connected, blah blah blah. I have to suppress those nodes so I can get through the program.

How can I get the grippers to be detected?

![image](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/2X/7/7974774433944fc952c43ebf4911b31ab1583053.png)

![image](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/2X/e/e967acf2c021591b91f87fd69df3fa978bbfaefa.png)

---

<div class="post-metadata">

### Author: ![anon80337847](https://avatars.discourse-cdn.com/v4/letter/a/47e85d/32.png) [@anon80337847](https://forum.universal-robots.com/u/anon80337847)
#### Post date: [November 11, 2021, 9:23pm UTC](https://forum.universal-robots.com/t/ursim-issues-robotiq-grippers-installed-but-not-working/15692/2 "2021-11-11T21:23:14Z")

</div>

I’m trying to do more programming from the office as well and have come up with 2 solutions that make it easier.

1. To get the grippers to work in URSIM I use the latest URSIM in virtual box, my grippers are connected via a USB - RS485 convertor.  
Assuming you have usb access setup properly on the sim (open terminal and type lsusb, you should see the FTDI adapter in the list) and the URCap installed, You just need to manually start the driver.  
Mine happens to be located /home/ur/ursim-current/GUI/felix-cache/bundle191/data/com/robotiq/urcap/gripper/impl/daemon/robotiq\_2f\_gripper\_driver.sh

Just search for it and run the robotiq\_2f\_gripper\_driver.sh script as root.

1. If I’m programming at the pendent or in the sim I’ll add the variable sim\_mode and initialize it to false, then add an operator assignment for sim\_mode. Then I move all my gripper actions(and any I/O that the sim doesn’t have) into IF statements checking the sim\_mode variable. If SIm\_mode = true, they are ignored, otherwise they run as they should.  
When I move to production I simply suppress the operator assignment and sim\_mode remains FALSE.

---

<div class="post-metadata">

### Author: ![anon507564](https://avatars.discourse-cdn.com/v4/letter/a/e480ec/32.png) [@anon507564](https://forum.universal-robots.com/u/anon507564)
#### Post date: [November 11, 2021, 10:14pm UTC](https://forum.universal-robots.com/t/ursim-issues-robotiq-grippers-installed-but-not-working/15692/3 "2021-11-11T22:14:24Z")

</div>

I’ve held off asking this because it sounds so stupid and I would be embarrassed for asking, but this is not the first time I’ve heard someone reference having physical grippers plugged in to their URSim.

To be clear, I am talking about the URSim that runs on my PC separate from my physical robots.

I have the robots out on the floor tending CNCs. I run them using the teach pendant.

I want to be able to simulate them in my office. Virtually. But my programs won’t run because it can’t find gripper 1 and gripper 2. The Robotiq URCap is installed in the simulator but they don’t show up in the Gripper tab and the programs don’t recognize them.

Am I mis-stating what URSim is or how I’m using it?

---

<div class="post-metadata">

### Author: ![anon80337847](https://avatars.discourse-cdn.com/v4/letter/a/47e85d/32.png) [@anon80337847](https://forum.universal-robots.com/u/anon80337847)
#### Post date: [November 11, 2021, 11:18pm UTC](https://forum.universal-robots.com/t/ursim-issues-robotiq-grippers-installed-but-not-working/15692/4 "2021-11-11T23:18:51Z")

</div>

I’m sorry, I thought you were trying to get the physical grippers working with the URSim.

I had the same initial problem but also had a spare set of grippers to connect. As far as I know, you need the grippers connected to run with the Robotiq URCap. You may be able to run some sort of serial server to trick the simulator into thinking a gripper is attached.

I have heard that you can use a modified/alternative URcap with the simulator but have not found it yet personally.

I’ve also moved to adding the sim\_mode flag I mentioned in my first post to all my programs I edit at my desk so I’m not sure I’ll invest much more into getting the URcap to work without a gripper installed. I’ll be sure to update if I do.

---

<div class="post-metadata">

### Author: ![anon507564](https://avatars.discourse-cdn.com/v4/letter/a/e480ec/32.png) [@anon507564](https://forum.universal-robots.com/u/anon507564)
#### Post date: [November 12, 2021, 2:40pm UTC](https://forum.universal-robots.com/t/ursim-issues-robotiq-grippers-installed-but-not-working/15692/5 "2021-11-12T14:40:58Z")

</div>

Ahhh, thank you for clearing that up. I like the solution you use (variable and if statements to use the grippers). I may try to do something like that.

Of course, I’d much rather UR fix the URSim so it will run the Robotiq URCap in the sim-only, but at least I know where to go next.

---

<div class="post-metadata">

### Author: ![krmi](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/krmi/32/1945_2.png) [@krmi](https://forum.universal-robots.com/u/krmi)
#### Post date: [November 17, 2021, 8:44pm UTC](https://forum.universal-robots.com/t/ursim-issues-robotiq-grippers-installed-but-not-working/15692/6 "2021-11-17T20:44:29Z")

</div>

Installing the URCaps in URSim will at least the change nodes from yellow to white. The nodes themselves are written by Robotiq, so perhaps you can reach out to them to see if they have a virtual version that will work without the hardware? My guess is they do some sort of check to see if they’re getting a signal from the gripper and throwing an error if they don’t get the right response.

---

<div class="post-metadata">

### Author: ![anon507564](https://avatars.discourse-cdn.com/v4/letter/a/e480ec/32.png) [@anon507564](https://forum.universal-robots.com/u/anon507564)
#### Post date: [November 17, 2021, 9:18pm UTC](https://forum.universal-robots.com/t/ursim-issues-robotiq-grippers-installed-but-not-working/15692/7 "2021-11-17T21:18:13Z")

</div>

The URCap is already installed in the URSim so the nodes are already white. It’s when it reads the gripper nodes that it throws the “Gripper not connected” error, so yes, it’s not getting the feedback.

I will contact Robotiq about it. Thanks for the feedback.