# UR Palletizing in Polyscope 5.12 only executes first item unless I add an external loop

**URL:** <https://forum.universal-robots.com/t/ur-palletizing-in-polyscope-5-12-only-executes-first-item-unless-i-add-an-external-loop/42363>\
**Category:** Technical Questions\
**Created:** [March 4, 2026, 10:32am UTC](https://forum.universal-robots.com/t/ur-palletizing-in-polyscope-5-12-only-executes-first-item-unless-i-add-an-external-loop/42363 "2026-03-04T10:32:46Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![timm](https://avatars.discourse-cdn.com/v4/letter/t/8e8cbc/32.png) [@timm](https://forum.universal-robots.com/u/timm)\
**Post date:** [March 4, 2026, 10:32am UTC](https://forum.universal-robots.com/t/ur-palletizing-in-polyscope-5-12-only-executes-first-item-unless-i-add-an-external-loop/42363/1 "2026-03-04T10:32:46Z")

</div>

Hello,

I am working with a **Universal Robots UR robot running Polyscope 5.12** and using the **Palletizing template**.

I created a simple palletizing program with a **grid pattern of 2 × 3 (6 items)**.  
Inside the palletizing node, I defined the pick and place sequence under **“At Each Item”** , which should repeat for every pallet position.

However, when I run the program **without any external loop** , the robot only executes the sequence **for the first item** and then the program stops.

What I observe:

- `Pallet_1_cnt` starts at **1**

- After placing the first item, `Pallet_1_cnt` becomes **2**

- The program then ends instead of continuing with item 2

If I add:

```auto
Loop 6 times
   Pallet_1

```

then the robot correctly places all **6 parts**.

From my understanding, the **“At Each Item”** node inside the Palletizing template should already act as the iteration over the pallet positions, so I expected the palletizing node to execute all items in one run.

My questions:

1. Is this the expected behavior in **Polyscope 5.12** , meaning that the Palletizing node only executes **one item per call**?

2. Should the palletizing node normally require an **external loop** to complete the pallet?

3. Why do some example videos show palletizing filling the whole pallet without an explicit loop?

For reference, my program structure is roughly:

```auto
Robot Program
   Gripper Activate
   Gripper Open
   MoveJ Waypoint_1
   Loop 6 times
       Pallet_1

```

And inside `Pallet_1`:

```auto
Patterns
   Grid_Pattern_1
      CornerItem_1
      CornerItem_2
      CornerItem_3
      CornerItem_4

Layers
   At Each Item
       MoveJ Waypoint_3
       MoveL Waypoint_2
       Gripper Close
       ...

```

Any clarification on the intended behavior of the Palletizing node in Polyscope 5.12 would be appreciated.

Thanks!UR

 ![UR1](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/2X/e/e454dbf12fee6e3d4a0445a578f61acdc37f2666.jpeg)

 ![UR2](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/2X/3/37f15b63809e8fc25de49ff548ebc3fc334832a6.jpeg)

 ![UR3](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/2X/f/ff6f711fae7e833304ef5c5df34354e7f275c41b.jpeg)

---

<div class="post-metadata">

**Author:** ![efn](https://avatars.discourse-cdn.com/v4/letter/e/35a633/32.png) [@efn](https://forum.universal-robots.com/u/efn)\
**Post date:** [March 5, 2026, 6:07am UTC](https://forum.universal-robots.com/t/ur-palletizing-in-polyscope-5-12-only-executes-first-item-unless-i-add-an-external-loop/42363/2 "2026-03-05T06:07:31Z")

</div>

That is indeed how the UR robot is intended to be used. By default, it will loop the whole sequence forever, so you must have disabled this function yourself.

The function can be found by highlighting the “Robot Program” line and going to the Command tab. At the bottom you will find the function for looping the sequence forever.

 ![image](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/2X/5/54b37c901b20266477b744791a1f95991ea20f1a.png)

The palletizing template is meant to be set up at just the first item location and only for either palletizing or depalletizing your items. You will need a sequence outside either before or after (usually both) for what to do with the items before/after.  
A quick look at your sequence would indicate you have misunderstood the above. 🙂

---

<div class="post-metadata">

**Author:** ![timm](https://avatars.discourse-cdn.com/v4/letter/t/8e8cbc/32.png) [@timm](https://forum.universal-robots.com/u/timm)\
**Post date:** [March 5, 2026, 6:39am UTC](https://forum.universal-robots.com/t/ur-palletizing-in-polyscope-5-12-only-executes-first-item-unless-i-add-an-external-loop/42363/3 "2026-03-05T06:39:53Z")

</div>

Thank you for the explanation.

I did try enabling **“Program Loops Forever”** , and in that case the palletizing sequence runs correctly through all 6 positions. However, the program then immediately starts again from the beginning and continues placing parts beyond the intended pallet capacity.

What I actually need is for the robot to **fill the pallet once (6 items in my case) and then stop**. Therefore, it seems necessary to add a condition at the end of the loop, for example checking when the pallet counter reaches the total number of items and then stopping the program.

So effectively the structure would be something like:

```auto
Loop
   Pallet_1
   If Pallet_1_cnt >= Pallet_1_tct
       Halt

```

From what I understand now, the palletizing template executes one item per program cycle and the iteration must be handled by the program loop.

I realize now that using a loop for palletizing is actually common on other robot platforms as well. My confusion came from assuming that the UR palletizing template might internally handle the full pallet sequence automatically, since it appears quite advanced compared to what I initially expected.

Thanks again for the clarification.

---

<div class="post-metadata">

**Author:** ![timm](https://avatars.discourse-cdn.com/v4/letter/t/8e8cbc/32.png) [@timm](https://forum.universal-robots.com/u/timm)\
**Post date:** [March 5, 2026, 6:52am UTC](https://forum.universal-robots.com/t/ur-palletizing-in-polyscope-5-12-only-executes-first-item-unless-i-add-an-external-loop/42363/4 "2026-03-05T06:52:46Z")

</div>

You mentioned that the issue might be related to the pick sequence before the palletizing node, but that part is already implemented in my program. I already have the **pick sequence placed before the palletizing operation**.

So that part is working as intended. The only issue I am currently facing was with the **loop behavior**

---

<div class="post-metadata">

**Author:** ![efn](https://avatars.discourse-cdn.com/v4/letter/e/35a633/32.png) [@efn](https://forum.universal-robots.com/u/efn)\
**Post date:** [March 5, 2026, 6:53am UTC](https://forum.universal-robots.com/t/ur-palletizing-in-polyscope-5-12-only-executes-first-item-unless-i-add-an-external-loop/42363/5 "2026-03-05T06:53:25Z")

</div>

No problem.

The palletizing template has a function for adding a sequence after the last item has been placed/picked. 🙂 I personally use this to set a variable to True telling a later sequence that it is finished.