I’m using SDK 1.7.0.
In the “com.ur.urcap.examples.tooliocontrol” example, I modified the line below:
private static final BuadRate REQUIRED_BAUDRATE = BaudRate.BAUD_2M
The REQUIRED_BAUDRATE was changed from 2M to 57600
private static final BuadRate REQUIRED_BAUDRATE = BaudRate.BAUD_57600
However, when I checked the result, it was set to 38400.
It works well when set to 1M.
@jbm Is it bug?