I need the times from the new Timer function.
When I need the Value from the Timer, I write with the script function “textmsg” the values in the protocol. It would be very useful, when there is a check button in the Timer function. When active then write the value and the name from the Timer in the protocol.