# Switch back to Remote Control from another operational mode without Teach Pendant

**URL:** <https://forum.universal-robots.com/t/switch-back-to-remote-control-from-another-operational-mode-without-teach-pendant/18048>\
**Category:** Technical Questions\
**Created:** [December 8, 2021, 10:05am UTC](https://forum.universal-robots.com/t/switch-back-to-remote-control-from-another-operational-mode-without-teach-pendant/18048 "2021-12-08T10:05:38Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![yann.devisscher](https://avatars.discourse-cdn.com/v4/letter/y/a88e57/32.png) [@yann.devisscher](https://forum.universal-robots.com/u/yann.devisscher)\
**Post date:** [December 8, 2021, 10:05am UTC](https://forum.universal-robots.com/t/switch-back-to-remote-control-from-another-operational-mode-without-teach-pendant/18048/1 "2021-12-08T10:05:38Z")

</div>

Hi everybody

Setup:  
The system I’m working with, doesn’t have a Teach Pendant installed.  
Polyscope version 5.11

I’m dealing with the following issue:  
My problem starts when switching to Manual mode (using I/O) after being in Remote Control mode, because it is not possible to return back to Remote Control. The I/O only offers switching between Manual and Automatic mode. I need to switch to Manual mode, because of safety and freedrive capabilities.

Question:  
Is there an option to return back to Remote Control using I/O, Profinet, TCP/IP a bash file or python?

My opinion:  
If it is possible to switch to Manual mode from the Remote Control mode using the I/O, then it should be possible to use the same approach to get back to Remote Control mode.

Please let me know, if there is a workaround for my issue. Thanks.

---

<div class="post-metadata">

**Author:** ![bba](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/bba/32/555_2.png) [@bba](https://forum.universal-robots.com/u/bba)\
**Post date:** [December 8, 2021, 3:24pm UTC](https://forum.universal-robots.com/t/switch-back-to-remote-control-from-another-operational-mode-without-teach-pendant/18048/2 "2021-12-08T15:24:45Z")

</div>

Hi,  
I’m afraid there is no way to do what you desire. The reason is that this functionality is driven by an ISO safety standard for industrial robots and how remote/local mode should work. IF the remote client could send a command to switch the robot from local to remote (and then also presumably start the robot moving) this would create a safety hazard to a local user who might be holding the teach pendant (as an example) and being close to the robot as it unexpectedly starts moving. The best option for you is to always keep the robot in remote mode.

---

<div class="post-metadata">

**Author:** ![yann.devisscher](https://avatars.discourse-cdn.com/v4/letter/y/a88e57/32.png) [@yann.devisscher](https://forum.universal-robots.com/u/yann.devisscher)\
**Post date:** [December 8, 2021, 4:02pm UTC](https://forum.universal-robots.com/t/switch-back-to-remote-control-from-another-operational-mode-without-teach-pendant/18048/3 "2021-12-08T16:02:20Z")

</div>

Thank you very much for the information, but I seriously don’t see the hazard.

Because:

1. there isn’t a Teach Pendant connected
2. if the user would connect a Teach Pendant while a program is active, the robot would go into Fault and stay that way, because the Safety configuration doesn’t correspond with the hardware configuration. For the robot to work without Teach Pendant, the safety installation has to configured previously (Hardware \> Teach Pendant → None).

I think this is a feature that should be included in future releases, at least when working with a Teach Pendant Free setup.

---

<div class="post-metadata">

**Author:** ![anon39314409](https://avatars.discourse-cdn.com/v4/letter/a/f9ae1b/32.png) [@anon39314409](https://forum.universal-robots.com/u/anon39314409)\
**Post date:** [October 28, 2022, 7:05am UTC](https://forum.universal-robots.com/t/switch-back-to-remote-control-from-another-operational-mode-without-teach-pendant/18048/4 "2022-10-28T07:05:21Z")

</div>

Hello, how did you go into remote control without the teach pendant?

---

<div class="post-metadata">

**Author:** ![yann.devisscher](https://avatars.discourse-cdn.com/v4/letter/y/a88e57/32.png) [@yann.devisscher](https://forum.universal-robots.com/u/yann.devisscher)\
**Post date:** [November 8, 2022, 7:45am UTC](https://forum.universal-robots.com/t/switch-back-to-remote-control-from-another-operational-mode-without-teach-pendant/18048/5 "2022-11-08T07:45:09Z")

</div>

You have to activate the remote control mode first, before dettaching the Teach Pendant. Another option is to access the Controller using TightVNC and activating the remote control mode from there.

Apparently, it is not possible to activate the remote control mode directly over the Dashboard, due to safety reasons.

I hope this info helps.