Storage capacity of a robot

Hello guys!

Would anyone know what t is the HD storage capacity of a Universal Robot?
CB and e-series probably do not have the same HD capacity to store programs, so a simple estimation would be fine.

I’ve never had the need to free space by deleting programs or something like that. As I said, it’s just a curiosity… :))

Looks like the standard SD card on these machines is 4GB - not sure how much is available for programs:

E-SERIES SD CARD

This article contains information about the different SD card used on e-Series Robots with its relative spare part numbers

Last modified on Dec 15, 2022

[](javascript:window.print())

  • 170010 SCD Card 4Gb SLC:

    • This shall be ordered if customer wants to have an empty SCD card without SW and SN.
  • 170013 - SCD Card 4Gb SLC incl. SW pre 2020:

    • This shall be ordered if the customer wants a SCD card with a specific SW versions installed and with a SN printed for robots Before 2020.
  • 170014 - SCD Card 4Gb SLC incl. SW 2020 forward:

    • This shall be ordered if the customer wants a SCD card with a specific SW versions installed and with a SN printed for robots From 2020 forward. This is NOT compatible with with robots produced before 2020.