what confused me for a while is that when i load a generated Script File from a Program with the Script Node it gets wrapped in the Robot Program like
def Program():
... init Stuff ...
$ 1 ProgramNode:
def Program():
... init Stuff...
$ 1 ProgramNode:
... original Program ...
end
end
which always leads to an Error because of duplicate node Numbers.
i need to delete these node references so this is why i’m asking for a feature to auto-unwrap the scripts or the ability to load scripts as a Program.
The Purpose of this would be to use cross-platform scripts with different Firmware Versions and robot types (e/CB-Series).