Hi,
I have a program node composed of two buttons and a textfield. Whenever I press the buttons their callback is invoked storing some parameters inside the DataModel.
undoRedoManager.recordChanges(new UndoableChanges() {
@Override
public void executeChanges() {
model.set("param", value);
}
});
The data is stored and I can press the save icon (floppy disk). The problem happens when I change the textfield value the onOk() callback is invoked and the param is stored on the dataModel but the save icon is still greyed out and I can’t trigger the program save.
I tried on the simulator and it works there. Any suggestion?
Thank you
The other odd thing is that undo/redo buttons don’t see the setting of the text of a JTextField.
In a URCap of mine I use both an KeyboardInputCallback<Integer>
and a KeyboardInputCallback<Double>
. The save button and undo/redo buttons both notice the change when an integer keyboard is called, but not when a double keyboard is called.
The code for both keyboards is identical, here is the code from onOk
for both:
Double keybaord:
@Override
public void onOk(Double, value)
{
myView.getDoubleTextField().setText(Double.toString(value));
model.set("double", value);
}
Integer Keyboard:
@Override
public void onOk(Integer, value)
{
myView.getIntegerTextField().setText(Integer.toString(value));
model.set("integer", value);
}
Certainly from this code I suspect that this is a bug with how polyscope triggers undoable changes?
Though it is worth noting that model.set(String, value)
is still triggering isDefined()
just fine
EDIT: putting an undoredoManager
inside onOk()
has no effect.
Hello, Sam.
Unfortunately I wasn’t able to find one.
Maybe someone can investigate this further.
Thanks,
Federico