Sanding cobot precision

Good evening,

I’m working on a wood sanding application using a UR cobot, Mirka 350s tool and an FT sensor which has a resolution near 0.1N, where my sanding force is 10-20N. I’m not sure which UR to choose, 5 or 10, because i’m not sure how sanding vibrations will affect the robot corrections. I wrote here some process values to emphasize that my application requires some precision. I’m inclined to go with 10, as it can have a higher rigidity than smaller one. What do you think ? If someone had something similar, could you tell me if UR5 can do the job ?. Thank you in advance:)

UR10 (UR12e) will give you much more flexibility from a reach perspective anyway so I suggest that.

Maybe consider the UR16e? It’s the joint sizes of the UR10e with the reach of a UR5e. So it will definitely be more resistant to vibrations and the reach should be okay, too.

But it is indeed important to isolate the tool as much as possible from the robot arm. I have seen applications before that use an external FT sensor such as the Robotiq FT-300.
The built-in FT sensor is not as precise as the FT-300, and it might be less sensitive to vibrations, as well.

are you sure about that? the ft sensor in the UR is an ft-300…

Yes, but a modified one. :slight_smile: You can check the specs between the dedicated one and the built-in one.