# Rx, Ry and Rz in Real Time Communication

**URL:** <https://forum.universal-robots.com/t/rx-ry-and-rz-in-real-time-communication/1050>\
**Category:** Robot Communication\
**Created:** [August 9, 2017, 8:34pm UTC](https://forum.universal-robots.com/t/rx-ry-and-rz-in-real-time-communication/1050 "2017-08-09T20:34:25Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![Felipe\_Nascimento](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/felipe_nascimento/32/452_2.png) [@Felipe\_Nascimento](https://forum.universal-robots.com/u/Felipe_Nascimento)\
**Post date:** [August 9, 2017, 8:34pm UTC](https://forum.universal-robots.com/t/rx-ry-and-rz-in-real-time-communication/1050/1 "2017-08-09T20:34:25Z")

</div>

Hey there!

Simple question but I couldn’t find the answer. When I use the Realtime Interface (port 30003),  
I can get the _Tool Vector Actual_ and the _Tool Vector Target_ Positions, which gives me the 6d Vector (x, y, z, rx, ry, rz). The problem is, the rx, ry and rz that I receive are not equal or even similar to the ones I can see in the Interface.

What exactly they represent? Is there a way to get the RPY orientation of the tool via the Realtime Interface TCP/IP?

Example of what I mean

In the Interface (relative to base):

```
         x = 573.32 mm
         y = -377.45 mm
         z = 110.4 mm

         Rotation Vector (rad)
         Rx = 1.656 
         Ry = -3.893
         Rz = -1.859

         RPY (rad)
         Rx = 0.154
         Ry = 1.485
         Rz = 0.973

```

The Tool vector I receive

```
         x = 0.5733132233401346
         y = -0.37745289619949307
         z = 0.11039638592902691

         Rx = -0.5957311311260479
         Ry = 1.4005856604020908
         Rz = 0.6689512228953933

```

The (x, y, z) is ok, but I can’t figure the (rx, ry, rz).

Thanks in advance.

---

<div class="post-metadata">

**Author:** ![mmi](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/mmi/32/691_2.png) [@mmi](https://forum.universal-robots.com/u/mmi)\
**Post date:** [August 14, 2017, 9:50am UTC](https://forum.universal-robots.com/t/rx-ry-and-rz-in-real-time-communication/1050/2 "2017-08-14T09:50:51Z")

</div>

Can it be that you’re decoding angles incorrectly?  
It should correspond to what you see on the move tab, and value returned by get\_actual\_tcp\_pose().  
rx,ry,rz are angles relative to base feature corrected by tcp rotation.  
So if tcp rotation offset == (0, 0, 0), then (rx, ry) == (0, 0) when tool flage is pointing in base z-axis direction.

---

<div class="post-metadata">

**Author:** ![jbm](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/jbm/32/614_2.png) [@jbm](https://forum.universal-robots.com/u/jbm)\
**Post date:** [August 14, 2017, 3:23pm UTC](https://forum.universal-robots.com/t/rx-ry-and-rz-in-real-time-communication/1050/3 "2017-08-14T15:23:04Z")

</div>

Also check out [this topic](http://forum.universal-robots.com/t/discrepancy-of-pose-from-30002-and-pendant-reading/238).

---

<div class="post-metadata">

**Author:** ![Felipe\_Nascimento](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/felipe_nascimento/32/452_2.png) [@Felipe\_Nascimento](https://forum.universal-robots.com/u/Felipe_Nascimento)\
**Post date:** [August 15, 2017, 7:47pm UTC](https://forum.universal-robots.com/t/rx-ry-and-rz-in-real-time-communication/1050/4 "2017-08-15T19:47:28Z")

</div>

I checked the topic and it looks like the position is the same but with other axis-angle representation (like the topic suggested, but in this case its not just a pi rotation), but when I command the robot to move (with _movel_) to the position returned by the RTDE, it says it’s a singularity.

The same applies when I try to apply the angles direct in the pendant. It’s a reacheble position exactly where it’s supposed to be in the pendant interface, but when I set it to move, it says it’s a singularity.

For now, I’ll try to work with the joint angles instead.

---

<div class="post-metadata">

**Author:** ![SonglinCai](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/songlincai/32/478_2.png) [@SonglinCai](https://forum.universal-robots.com/u/SonglinCai)\
**Post date:** [August 18, 2017, 9:18pm UTC](https://forum.universal-robots.com/t/rx-ry-and-rz-in-real-time-communication/1050/5 "2017-08-18T21:18:21Z")

</div>

Singularity means robot close to its kinematic singularity rather than they cannot reach it actually. Robot vector is not unique to a given reorientation so although they have different appearances, they are indeed the same. Check out via wiki on rotation vector.