# Ros2\_grasp\_library

**URL:** <https://forum.universal-robots.com/t/ros2-grasp-library/24459>\
**Category:** ROS\
**Created:** [October 18, 2022, 9:07am UTC](https://forum.universal-robots.com/t/ros2-grasp-library/24459 "2022-10-18T09:07:39Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![anon30780346](https://avatars.discourse-cdn.com/v4/letter/a/dc4da7/32.png) [@anon30780346](https://forum.universal-robots.com/u/anon30780346)\
**Post date:** [October 18, 2022, 9:07am UTC](https://forum.universal-robots.com/t/ros2-grasp-library/24459/1 "2022-10-18T09:07:39Z")

</div>

I want to use the [ros2\_grasp\_library](https://intel.github.io/ros2_grasp_library/docs/doc/overview.html). But I’m a bit confused about the requirements of this Library.

However i tried to install it anyways. I’m using ROS2 Humble and MoveIt2 on my Ubuntu 22.04.  
There i created a new folder `~/workspace/pick_and_place_ros_ur/src` where i cloned the [github repository](https://github.com/intel/ros2_grasp_library.git) to.  
When i try to build it i get following error:

```auto
colcon build --base-paths src/ros2_grasp_library/grasp_apps/fixed_position_pick
Starting >>> fixed_position_pick
--- stderr: fixed_position_pick                         
CMake Error at CMakeLists.txt:35 (find_package):
  By not providing "Findrobot_interface.cmake" in CMAKE_MODULE_PATH this
  project has asked CMake to find a package configuration file provided by
  "robot_interface", but CMake did not find one.

  Could not find a package configuration file provided by "robot_interface"
  with any of the following names:

    robot_interfaceConfig.cmake
    robot_interface-config.cmake

  Add the installation prefix of "robot_interface" to CMAKE_PREFIX_PATH or
  set "robot_interface_DIR" to a directory containing one of the above files.
  If "robot_interface" provides a separate development package or SDK, be
  sure it has been installed.

```

My [Universal\_Robots\_ROS2\_Driver](https://github.com/UniversalRobots/Universal_Robots_ROS2_Driver) is in `~/workspace/ros_ur_driver`.

Do i need to install the library to a different location?

What requirements do i need to run this library?  
In the [issues](https://github.com/intel/ros2_grasp_library/issues) sections, there are some unanswered questions about the UR\_Driver, MoveIt Version, ROS2 Version.