# Problem with getUserDefinedRobotPosition / joint positions

**URL:** <https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981>\
**Category:** Technical Questions\
**Tags:** bugs\
**Created:** [October 24, 2018, 10:02am UTC](https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981 "2018-10-24T10:02:57Z")\
**Posts on this page:** 8\
**Page:** 1

<div class="post-metadata">

**Author:** ![anon12495347](https://avatars.discourse-cdn.com/v4/letter/a/779978/32.png) [@anon12495347](https://forum.universal-robots.com/u/anon12495347)\
**Post date:** [October 24, 2018, 10:02am UTC](https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981/1 "2018-10-24T10:02:57Z")

</div>

Problem: the shown 'Set Waypoint’is different form ‘Edit pose’ and both different from ‘shown picture’.  
Set Waypoint shows:  
 ![image](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/1X/8cf4541b0e1a9a63ca5b1cb28a15f30329d5cc2b.png)  
Edit pose shows:

 ![editpose](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/1X/6425a72601b2268f3d2980c2059ad17379d05b93.png)  
‘summary’ picture shows:  
 ![spicture](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/1X/83a63ee57e54fa62e805fceae41f7b5f6bbcdafd.png)

Example show above is of EllipsPos4. However, all saved waypoints do have similar mismatch problem .

Reproduce, use URCAP Ellipse Swing. Problem occurs if TCP is not 0,0,0,0 .  
Set tcp to:  
 ![tcp](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/1X/cbe2ee6edb3e57387ac0567eb7165933ddd66161.png)  
Note that the difference between ‘Set waypoint’ and ‘Edit pose’ is exactly the values of the TCP !. The shown ‘summary picture’ seems to have the correct TCP but having another, not correct pose.

When going tho ‘Set Waypoint’ of one of the mismatched waypoints, and click OK, now all 3 data views are in sync with what is shown in ‘Set Waypoint’

Using version 3.7.0

---

<div class="post-metadata">

**Author:** ![m.birkholz](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/m.birkholz/32/7084_2.png) [@m.birkholz](https://forum.universal-robots.com/u/m.birkholz)\
**Post date:** [October 26, 2018, 10:09am UTC](https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981/2 "2018-10-26T10:09:43Z")

</div>

Thank God i’m not the only one facing this odd Bug.  
related to [Calling Pose from URCap generated Waypoint misses TCP Offset](https://forum.universal-robots.com/t/calling-pose-from-urcap-generated-waypoint-misses-tcp-offset/2275)

i’m also having issues with URCap generated Waypoint that have a wrong inverse kinematic.  
This is still present on the latest UR10e-Series!

@jbm please fix this

---

<div class="post-metadata">

**Author:** ![jbm](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/jbm/32/614_2.png) [@jbm](https://forum.universal-robots.com/u/jbm)\
**Post date:** [October 26, 2018, 12:28pm UTC](https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981/3 "2018-10-26T12:28:31Z")

</div>

Is the issue only related to the graphics?  
Or is the wrong (further away) joint position also used when running the program or using “Move here”?

---

<div class="post-metadata">

**Author:** ![anon12495347](https://avatars.discourse-cdn.com/v4/letter/a/779978/32.png) [@anon12495347](https://forum.universal-robots.com/u/anon12495347)\
**Post date:** [October 30, 2018, 7:47am UTC](https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981/4 "2018-10-30T07:47:16Z")

</div>

Yes, it is also the wrong joint position when running or using ‘Move here’. So, not only in graphics shown.

---

<div class="post-metadata">

**Author:** ![anon12495347](https://avatars.discourse-cdn.com/v4/letter/a/779978/32.png) [@anon12495347](https://forum.universal-robots.com/u/anon12495347)\
**Post date:** [October 31, 2018, 8:42am UTC](https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981/5 "2018-10-31T08:42:42Z")

</div>

Is there any progress perhaps on this issue ? We are struggling now in our URCAP development. Thanks .

---

<div class="post-metadata">

**Author:** ![jbm](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/jbm/32/614_2.png) [@jbm](https://forum.universal-robots.com/u/jbm)\
**Post date:** [November 14, 2018, 11:46am UTC](https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981/6 "2018-11-14T11:46:34Z")

</div>

We are investigating the issue.

---

<div class="post-metadata">

**Author:** ![dmartin](https://avatars.discourse-cdn.com/v4/letter/d/c4cdca/32.png) [@dmartin](https://forum.universal-robots.com/u/dmartin)\
**Post date:** [July 9, 2019, 4:40pm UTC](https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981/7 "2019-07-09T16:40:12Z")

</div>

Thank you @m.birkholz for pointing out this post for me. I am facing the same problem.

_Note: I was able to separate another bug that at first seemed to be part of the same. It is covered in [Capturing pose with a button, questions and troubles](https://forum.universal-robots.com/t/capturing-pose-with-a-button-questions-and-troubles/4678)_.

I’m working in the URCap for a control disc with 2 buttons that goes in between the wrist and the tool.  
• One button is for freedrive.  
• The other is for recording waypoints.

I’m having trouble creating the right pose for this waypoints.

- I receive well the **pose** and **joint positions** via RT (30003 port). This data **includes the TPC**.

- But, when I use `createFixedPositionConfig` I’ve come to the conclusion this method is expecting the **pose without tool** , just at the wrist.

How I found out? Similarly to other entries in this post, I see this method **is working fine with TCP = 0, 0, 0, 0, 0, 0**.

But with any different TCP is not.

I’ve calculated ‘error’ XYZ distance and it matches to decimals with the TPC XYZ distance from the wrist.  
The orientation angles I didn’t check it mathematically, but seem to me to be matching the TCP orientation.

Two ways to see it:

1. **It is a bug** : @jbm Then, please UR team, fix it asap 😬  
The `createFixedPositionConfig` method should use the TPC for calculations.  
Probably adding optional parameters to the method would do. Should include:

2. **It is intended to be like this** , not taking the TPC into consideration: Then, we need to have **pose\_trans** and **pose\_inv** methods in Java asap. Can you help @jbm 😬  
This would allow us (non matrix mathematisian experts in general, at least not me) to add a given TPC to have the rigth pose.  
There’s a post on this too: [Pose\_trans and pose\_inv functions in URCap - #5 by dmartin](https://forum.universal-robots.com/t/pose-trans-and-pose-inv-functions-in-urcap/1257/5)

Thanks a lot folks!!

---

<div class="post-metadata">

**Author:** ![m.birkholz](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/m.birkholz/32/7084_2.png) [@m.birkholz](https://forum.universal-robots.com/u/m.birkholz)\
**Post date:** [July 9, 2019, 5:24pm UTC](https://forum.universal-robots.com/t/problem-with-getuserdefinedrobotposition-joint-positions/2981/8 "2019-07-09T17:24:50Z")

</div>

The issue comes up when the tcp rotation is other than x,y,z,0,0,0. the api generated waypoints do have the tcp offset tho. See [Here](https://forum.universal-robots.com/t/set-tool-center-point-to-use-active-tcp-inside-custom-urcap-waypoint-node/1914). This was implemented a year ago and should work. To prevent it from calculating the false inverse kinematics we calculated the rotation manually (rx = -0.58,ry=0,rz=0). After that the bug no longer occurs tho it is **not possible to move the robot in the tool space** correctly😉