# PositionParameters / Wrong Pose using WaypointNodeFactory with specific TCP Rotation

**URL:** https://forum.universal-robots.com/t/positionparameters-wrong-pose-using-waypointnodefactory-with-specific-tcp-rotation/6982
**Category:** Technical Questions
**Tags:** bugs
**Created:** [April 16, 2020, 12:56pm UTC](https://forum.universal-robots.com/t/positionparameters-wrong-pose-using-waypointnodefactory-with-specific-tcp-rotation/6982 "2020-04-16T12:56:49Z")
**Posts on this page:** 1
**Showing post:** 7

<div class="post-metadata">

### Author: ![m.birkholz](https://sea2.discourse-cdn.com/flex020/user_avatar/forum.universal-robots.com/m.birkholz/32/7084_2.png) [@m.birkholz](https://forum.universal-robots.com/u/m.birkholz)
#### Post date: [April 28, 2020, 5:50am UTC](https://forum.universal-robots.com/t/positionparameters-wrong-pose-using-waypointnodefactory-with-specific-tcp-rotation/6982/7 "2020-04-28T05:50:34Z")

</div>

The Issue with the Kinematics is a wrong Pose Result after using the API Interface WaypointNodeFactory. This can be reproduced on the Ellipse Example as well as the integrated Palletizing Node with the Pick/Place Waypoint Assistent.

You can try the following to reproduce the bug:

1. Setup a home pose with axis postions(deg) 0,-90,-90,-56.56,90,0 - the robot tool flange now points down to the base plane.

2. move the robot to the home position and set the tcp orientation with the asisstant with this pose relative to the base plane - the output should sth like 1.88,-1.88,0.5676:  

3. set a tcp offset of about 300 mm to z

4. select the ellipse urcap and program the center point to the home pose

5. the the waypoint node should now display the wrong Pose:

---

_[View the full topic](https://forum.universal-robots.com/t/positionparameters-wrong-pose-using-waypointnodefactory-with-specific-tcp-rotation/6982)._