# PopUpMessage in Primary Interface

**URL:** <https://forum.universal-robots.com/t/popupmessage-in-primary-interface/14786>\
**Category:** Robot Communication\
**Created:** [June 8, 2021, 1:20pm UTC](https://forum.universal-robots.com/t/popupmessage-in-primary-interface/14786 "2021-06-08T13:20:53Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![anon8207419](https://avatars.discourse-cdn.com/v4/letter/a/82dd89/32.png) [@anon8207419](https://forum.universal-robots.com/u/anon8207419)\
**Post date:** [June 8, 2021, 1:20pm UTC](https://forum.universal-robots.com/t/popupmessage-in-primary-interface/14786/1 "2021-06-08T13:20:53Z")

</div>

Hi,

I’ve been working for a few weeks on an application that connects via socket through the primary interface with a CB3 robot (currently, i am using ursim 3.14). Now I am trying to receive “PopUpMessages”:

int messageSize  
unsigned char messageType=MESSAGE\_TYPE\_ROBOT\_MESSAGE=20  
uint64\_t timestamp  
char source  
char robotMessageType=ROBOT\_MESSAGE\_TYPE\_POPUP=2  
unsigned int requestId  
unsigned int requestedType  
bool warning  
bool error  
bool blocking  
uint8\_t popupMessageTitleSize  
charArray popupMessageTitle  
charArray popupTextMessage

I use the attached documents on [Remote Control Via TCP/IP - 16496](https://www.universal-robots.com/articles/ur/interface-communication/remote-control-via-tcpip/) to know the structure of each package.

While trying to receive this type of package, I noticed that robotMessageType value of PopupMessage is 9 instead of 2. Is that possible?

I know that there is another type of MESSAGE\_TYPE\_ROBOT\_MESSAGE that has robotMessageType = 9 (RequestValueMessage), but it isn’t this one, it is a PopupMessage, because i can get all the information of PopupMessages showed above.

Maybe I am misunderstanding something related with the documentation, correct me if it is the case.

Also, I would like to point that the ValueTypes in excel are not updated, while in the pdf file they are.

Thank you for your time!