Pim 60 with Ur10

Hi everyone I have this problem.
Using the Pim 60(camera) saves me the position values ​​and whether or not it recognizes the object in the following variables “SICK_objLocated, SICK_Pos” which recognizes them as global variables.

When using them/saving the x,y,z, using the assignment function, they do not appear in the variable drop-down panel. Could you give me some option to be able to operate with them, even if it is an alternative method such as using a script or some other function.

the main problem is how can i use that globals variables and save them in other local variables.

Have you tried just writing them out in the Expression editor? Should work if they’re declared by the URCap beforehand. :slight_smile:
You can for example assign them to another variable in PolyScope making them “visible”.

how did you tyoe it, on the expression block i cant type , only select functions,numbers,varieables asigned before…

You have a keyboard layout somewhere on that screen, which switches the numeric buttons to letters. :slight_smile: Its placement varies on some older CB3 versions.

1 Like

i got it . truthly thanks for help me . There is any method to show te value of one variable. i have just done what you said to me but i want to verify if that value is correctly saved.