Moment of inertia UR3 UR5 UR10

I am building a robot mobility platform and I need to understand the maximum moment of inertia for all three robots. I thought I would ask here first and if the information is unavailable, then I will calculate and hope that my calculations are correct.
Thanks,
Jerry Stokely

These values are stored on each robot in .urcontrol/urcontrol.conf file. Look for [Link] section. Link lengths are defined as a part of [DH] parameters.
It slightly varies over robot generations, so you should download values for robot that you actually use.

MMI,
Thanks for the information, it was helpful
Jerry Stokely

This topic was automatically closed 2 days after the last reply. New replies are no longer allowed.