Memory Full Solution

I’m using UR3 with Robotiq Wrist Camera and Vacuum Grippers to pick and place objects (approximately 50 objects).
When I try to teach a new object I got some error message when I click on save icon (something like I can’t save).
After the save command, main program have 0MB and I can’t load this file along with installation file where I have snapshot position.

Linux free command show me this:
total used free shared buffers cached
Mem: 1,8G 1,8G 59M 0B 35M 345M

My question is regarding cleaning memory.
I have this path /dev/disk/by-uuid/… 1,8G 1,8G 0 100% / which is 100% used. Is this 1.8GB the internal memory of the teach pendant?

What could be the implications of this 100% occupancy percentage and what should be deleted to clean up and get out of this situation? What paths or folders are involved in this memory?

Hello Roxana,

You can go in program files and delete .old files. If the amount .old files are huge, you will clean up some space.

Hope this helps.
Giorgi