# Load capacity requirements for UR5e stands

**URL:** <https://forum.universal-robots.com/t/load-capacity-requirements-for-ur5e-stands/39092>\
**Category:** Technical Questions\
**Created:** [March 18, 2025, 3:01pm UTC](https://forum.universal-robots.com/t/load-capacity-requirements-for-ur5e-stands/39092 "2025-03-18T15:01:54Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![pablo](https://avatars.discourse-cdn.com/v4/letter/p/ad7895/32.png) [@pablo](https://forum.universal-robots.com/u/pablo)\
**Post date:** [March 18, 2025, 3:01pm UTC](https://forum.universal-robots.com/t/load-capacity-requirements-for-ur5e-stands/39092/1 "2025-03-18T15:01:55Z")

</div>

I’m working on designing a stand for a UR5e robot and I’m trying to understand the load capacity requirements for the stand. I see two sections in the UR5e user manual that appear to give conflicting or confusing information. I’m hoping someone here can help clarify the requirements.

First, section _6. Assembly, subpoint 2_ says:

> Mount the robot arm on a sturdy, vibration-free surface.  
> Verify the surface can withstand **at least 10 times the full torque of the base joint and**  
> **at least 5 times the weight of the robot arm.**

If I read that, and take the full torque of the base joint from [here](https://www.universal-robots.com/articles/ur/robot-care-maintenance/max-joint-torques-cb3-and-e-series/) to be 150 Nm and the weight of the robot to be 20.7 Kg (i.e. 203 N), then that would mean the stand would need to support up to 1,500 Nm of torque without specifying on which axis, and at least 1,015 N of vertical force.

Then on section _6.2. Dimensioning the Stand_, the following diagram and tables are provided. Here it appears Fz more or less matches the vertical force I calculated above, but the torque is about half as much in the worst case scenario Mxy and even less in the case of Mz. And this is already including a 2.5 safety factor according to the text above the table.

 ![image](https://us1.discourse-cdn.com/flex020/uploads/universal_robots/original/2X/9/96f75ca61220310807342864d30bb1ac0983881c.jpeg)

So this leaves me confused and wondering what are the correct load requirements, in particular in regards to torque, that the stand should be designed to support.

Any idea what are the correct requirements? Or perhaps I’m misunderstanding one of these sections and someone can help clarify which one and why?

Pablo C.

---

<div class="post-metadata">

**Author:** ![lois](https://avatars.discourse-cdn.com/v4/letter/l/5f8ce5/32.png) [@lois](https://forum.universal-robots.com/u/lois)\
**Post date:** [January 19, 2026, 5:18pm UTC](https://forum.universal-robots.com/t/load-capacity-requirements-for-ur5e-stands/39092/2 "2026-01-19T17:18:55Z")

</div>

I’m also interested in a more detailed definition of these loads.

In order not to the overdo the structural design of the stand, I would like to know :

Is this table to be treated as a combination? If not, what are the mitigating coefficients to be used in a worst case scenario for each load?

i.e. Mxy max load : 0.5Mz + 0.75Fz + Mxy + 0.75Fxy.

Thanks,

---

<div class="post-metadata">

**Author:** ![efn](https://avatars.discourse-cdn.com/v4/letter/e/35a633/32.png) [@efn](https://forum.universal-robots.com/u/efn)\
**Post date:** [January 20, 2026, 6:02am UTC](https://forum.universal-robots.com/t/load-capacity-requirements-for-ur5e-stands/39092/3 "2026-01-20T06:02:57Z")

</div>

I’ll share what I’ve experienced with the UR robots (as well as all other robots for that matter).

You want a stand that’s most likely far above those requirements mentioned in the article.  
What you should focus on is making a stand that is sturdy enough to prevent any vibrations caused by the robot arm movements to spread downwards and for the robot arm to be 100% still during operation.  
These vibrations can be damaging for the robot and cause protective stops etc.

Don’t be afraid of overdoing the stand. 🙂

---

<div class="post-metadata">

**Author:** ![lois](https://avatars.discourse-cdn.com/v4/letter/l/5f8ce5/32.png) [@lois](https://forum.universal-robots.com/u/lois)\
**Post date:** [February 27, 2026, 1:31pm UTC](https://forum.universal-robots.com/t/load-capacity-requirements-for-ur5e-stands/39092/4 "2026-02-27T13:31:08Z")

</div>

Unfortunately I have extreme weight limitations, the whole thing being lifted in the air. We would be okay with annoying protective stops if it means that we can keep under the weight limit.

I’ve had an idea about reducing the design loads by reducing the momentum limit, would you have an input on that?

> [@Reducing stand design loads by using a momentum limit or power limit](https://forum.universal-robots.com/t/reducing-stand-design-loads-by-using-a-momentum-limit-or-power-limit/42336):
>
> Hi there, I am designing a linear moving platform stand for a UR20. Basically a motorized carriage with four bearings on 2 rails. We have to stay under a weight limit for the whole thing, and that means light rails, light supports. At this point the maximum load applied to the stand/carriage is the one transmitted to the stand by the UR when it performs a category 0 stop under a worst-case scenario, per the UR20 manual (p50). ([Dimensioning the Stand](https://www.universal-robots.com/manuals/EN/HTML/SW5_20/Content/prod-usr-man/complianceUR20/H_g5_sections/mechanical_interface_g5/dimension_stand.htm)) Physically, it means that when the UR has a…