Universal Robots Forum

How to read network adapter's ip address within VMWare machine as ursim lock terminal in guest mode

How to open terminal or read out ip address within VMWare Machine as ursim lock terminal in guest mode.
I would like to ftp .urp file and test server-client application within ursim(client) and server,so that I could pre-program and test logic at home without real robot.

Inside the VM, e.g. the Starter Package, you can just run CTRL+ALT+T, which opens a terminal and try ifconfig to check your IP settings.
The admin password is easybot if needed at any point.

1 Like