i am developing a Plug-in, which contains 5 JSliders. All of them are updating the ProgramNode-Title individually.
Unfortunately, the performance of my gui is suffering from that. The slider motion is really laggy.
The part draining on the performance is mainly this one (and getTitle()):
public void onSliderSelection(final int[] newValue)
{
undoRedoManager.recordChanges(new UndoableChanges() {
I got the problem.
I wrote my functions really poorly, each slider was triggering two for-loops(one in view and one in the contribution) resulting into this performance loss. The dataModel was invoked way to often.
View.class: Have a changelistener on all of the sliders…
slider.addChangeListener(new ChangeListener() {
@Override
public void stateChanged(ChangeEvent arg0) {
provider.get().onSliderSelection("nameOfSlider", valueOfTheSlider)
}
});
Contribution.class: make a switch case to decided which slider value to set as the title.
public void onSliderSelection(final String nameOfSlider ,final int newValue)
{
undoRedoManager.recordChanges(new UndoableChanges() {
@Override
public void executeChanges() {
setMyModelBasedOnSliderValue(nameOfSlider, newValue)
}
});
}
Private setMyModelBasedOnSliderValue(String nameOfSlider, int inputValue) {
switchCase(nameOfSlider):
case(slider1)
model.setValue(inputValue)
case(slider2)
model.setValue(inputValue)
....etc...
}
By using switch case, it could be something like that. It would avoid looping. Hope it helped!
I tried it with switchcase but my jre version wouldnt allow strings as case values.
So i just gave every slider a key value on the view side. For the contribution, i left it as it is but without a for-loop.
Now it works bug- and lagfree.
In general, if there is a need for how to incorporate Swing GUI, then have a look at this article. on our getting started site. It contains example for swing components that are often use in developing a URCap.