# Emergency stop information from configurable Safety outputs

**URL:** <https://forum.universal-robots.com/t/emergency-stop-information-from-configurable-safety-outputs/29287>\
**Category:** Technical Questions\
**Created:** [June 29, 2023, 4:44am UTC](https://forum.universal-robots.com/t/emergency-stop-information-from-configurable-safety-outputs/29287 "2023-06-29T04:44:37Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![anon61096440](https://avatars.discourse-cdn.com/v4/letter/a/e36b37/32.png) [@anon61096440](https://forum.universal-robots.com/u/anon61096440)\
**Post date:** [June 29, 2023, 4:44am UTC](https://forum.universal-robots.com/t/emergency-stop-information-from-configurable-safety-outputs/29287/1 "2023-06-29T04:44:37Z")

</div>

Hello all,

I’m looking for a way to get the status of the emergency stop button at the PolyScope (Teach-Panel) from the configurable safety outputs.  
I know that it is possible to configure “Robot emergency stop”.  
The problem with this is, that if I send an emergency stop command to the robot, the robot will also send me an emergency stop, even if the emergency stop button is not pressed at all.  
I need a way to only get the emergency stop button so that I can evaluate the signal in my safety controller.

I hope someone can help me.

Tanks and kind regards,

-Stirni

---

<div class="post-metadata">

**Author:** ![eric.feldmann](https://avatars.discourse-cdn.com/v4/letter/e/94ad74/32.png) [@eric.feldmann](https://forum.universal-robots.com/u/eric.feldmann)\
**Post date:** [June 29, 2023, 1:59pm UTC](https://forum.universal-robots.com/t/emergency-stop-information-from-configurable-safety-outputs/29287/2 "2023-06-29T13:59:50Z")

</div>

What we’ve done in the past is just letting the robot’s E-Stop output be the last signal in the chain. Something like “E-Stops OK” is driven from the Robot outputs. In this way, if any external E-Stop were to be pressed, the Robot output would turn off (Estops not OK) and if all others are fine but the robot pendent EStop was pressed, you still lose E-Stops OK. You can do a little logic if you had to in the safety controller to isolate it at that point. If you have all external E-Stops good, but not E-Stops OK, then you know it’s the pendent E-Stop that is pressed.

---

<div class="post-metadata">

**Author:** ![anon61096440](https://avatars.discourse-cdn.com/v4/letter/a/e36b37/32.png) [@anon61096440](https://forum.universal-robots.com/u/anon61096440)\
**Post date:** [June 29, 2023, 2:30pm UTC](https://forum.universal-robots.com/t/emergency-stop-information-from-configurable-safety-outputs/29287/3 "2023-06-29T14:30:55Z")

</div>

Thank you for your response Eric.  
Its actually a good idea but does not work for me.  
I need to send a collected emergency stop signal to another machine.  
With this solution I would never have a “plain” signal because I always would have to acknoledge the error  
to check if the emergency stop still persists.  
 → I would turn in a circle and never be able to acknoledge the error.

Not a clean solution, but acceptable for me I did this:  
Collected emergency stop signal but without cobot e-stop.  
If I do not send this collected e-stop to cobot I evaluate if cobot sends me e-stop  
 → if yes, e-stop is pressed at teach pendant on cobot.  
 → I do not evaluate the signal if I already send e-stop to cobot

So in the worst case E-Stop 1 and E-Stop Cobot is pressed and I just get a message that E-Stop 1 is pressed.  
If then E-Stop 1 is acknoledged, then the message E-Stop cobot is pressed will be shown.

Like I said, not a clean solution but I can live with that.

Thanks for your support Eric!

-Stirni