# Access Standard and Configurable Outputs via RTDE

**URL:** <https://forum.universal-robots.com/t/access-standard-and-configurable-outputs-via-rtde/5249>\
**Category:** Robot Communication\
**Created:** [October 2, 2019, 12:22pm UTC](https://forum.universal-robots.com/t/access-standard-and-configurable-outputs-via-rtde/5249 "2019-10-02T12:22:40Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![fabricio.coelho2010](https://avatars.discourse-cdn.com/v4/letter/f/ad7895/32.png) [@fabricio.coelho2010](https://forum.universal-robots.com/u/fabricio.coelho2010)\
**Post date:** [October 2, 2019, 12:22pm UTC](https://forum.universal-robots.com/t/access-standard-and-configurable-outputs-via-rtde/5249/1 "2019-10-02T12:22:40Z")

</div>

Hello everyone,

I cannot access my digital outputs via RTDE., so, I have any doubts:

1 - There are two “functions” to access outputs? (standard\_digital\_output\_mask and standard\_digital\_output) .

2- Do they work the same way?

3- Can I choisse only one to use?

4- The variable’s type is UINT8. I must send a variable UINT8, for example, value = 127 (mask = 01111111). Is it correct?

5- I’m using the simulator, could this be the problem?

I can send my package via RTDE, I can set input registers but never set the outputs.

Thank you

---

<div class="post-metadata">

**Author:** ![fabricio.coelho2010](https://avatars.discourse-cdn.com/v4/letter/f/ad7895/32.png) [@fabricio.coelho2010](https://forum.universal-robots.com/u/fabricio.coelho2010)\
**Post date:** [October 2, 2019, 6:29pm UTC](https://forum.universal-robots.com/t/access-standard-and-configurable-outputs-via-rtde/5249/2 "2019-10-02T18:29:23Z")

</div>

Hello, I founded the solutions for my issues:

Standard\_digital\_output: Value to set the Ports (0 - False and 255 - True)  
Standard\_digital\_output\_mask: Mask with Ports that you want to enable or Disable

Example: I want enable Ports 2 and 3  
Standard\_digital\_output = 255  
Standard\_digital\_output\_mask = 10

10 is 00001100 on base 2