Please go to the Download Center, to get the latest Starter Package.
New to Java, Maven, Linux or URSim?
If you do not care which Java IDE you are using, or are not familiar with Linux, you can download this starter package.
The starter package includes a virtual Ubuntu image with:
- URSim (UR simulator with graphical user interface PolyScope)
- URCaps SDK (including sample URCap projects, the API and repository)
- Maven 3
- Eclipse Kepler Java IDE
All you need is a virtual machine software like VirtualBox or VMWare.
Instructions:
- Load the virtual image into your preferred virtual machine software
- Play the virtual machine
- Start Eclipse IDE.
Open a terminal (CTRL+ALT+T) and write:
cd eclipse/ ./eclipse
- Check out the loaded HelloWorld URCap project
- Import the MyDaemon to Eclipse.
File > Import > Maven > Existing Maven Projects > Next > Browse
Locate the MyDaemon sample in Home > urcap-sdk-1.0.0.7 > samples
Click OK and Finish - Build the HelloWorld URCap.
Open a terminal and write:
cd urcap-sdk-1.0.0.7/samples/com.ur.urcap.examples.helloworld/ mvn install
- Explore the IDE and URCaps SDK, and try to deploy the URCaps to the URSim.
Instructions and further help is found in the URCaps Tutorial enclosed in the SDK.
A new Starter Package is now available for:
URSim 3.3.0.145
URCaps SDK 1.0.0.7
(Download options in first post above)
A new Starter Package is now available for:
URSim 3.3.4.310
URCaps SDK 1.0.1.8
(Download options in first post above)
An FTP download option have now been added to the first post of this topic.
If you have had issues with direct download (could happen on slow or bad connections), please try the FTP option.
A new Starter Package is now available for:
URSim 3.4.0.39
URCaps SDK 1.1.0.76
(Download options in first post above)
Note:
The HelloWorld sample is made with the 1.0 API, while the two new samples are made with the 1.1 API to demonstrate the ability to create a URCap with active selection of API version.
A new Starter Package is now available for:
URSim 3.5.0.10584
URCaps SDK 1.2.41
(Download options in first post above)