Hello,
after I installed Linux Mint I am having trouble to install the URCap SDK, urcap-sdk-1.0.0.7
I like to use Linux Mint because there is more software available.
It´s the linuxmint-17.1-cinnamon-64bit- version
The error message is:
dpkg: error processing archive urtool/urtool3_0.3_amd64.deb (–install):
trying to overwrite ‘/opt/urtool-3.0/lib/libxmlrpc_server.so.3.33’, which is also in package libxmlrpc-c-ur 1.33.14
dpkg: error: subprocess paste was killed by signal (Broken pipe)
Errors were entcountered while processing:
urtoo/urtool3_0.3_amd64.deb
Done. Please log out and back in.
Is
This error is related to the installation of UR Tool chain.
Let me know if this fix does not solve it.
Hello Jacob,
finally I have the Hello World Demo running.
So these were my steps:
-
Use the URSim 3.30.145 Starter package
-
Change the ./install.sh file and comment the lines described in your fix with the ‘#’
#echo “Installing UR tool chain…”
#mvn install:install-file -Dfile=artifacts/commons-httpclient-3.1.0.0.jar -DgroupId=commons-httpclient -DartifactId=commons-httpclient -Dversion=3.1.0.0 -Dpackaging=jar -q
#mvn install:install-file -Dfile=artifacts/ws-commons-util-1.0.2.0.jar -DgroupId=org.apache.ws.commons.util -DartifactId=ws-commons-util -Dversion=1.0.2.0 -Dpackaging=jar -q
#mvn install:install-file -Dfile=artifacts/xmlrpc-client-3.1.3.0.jar -DgroupId=org.apache.xmlrpc -DartifactId=xmlrpc-client -Dversion=3.1.3.0 -Dpackaging=jar -q
#mvn install:install-file -Dfile=artifacts/xmlrpc-common-3.1.3.0.jar -DgroupId=org.apache.xmlrpc -DartifactId=xmlrpc-common -Dversion=3.1.3.0 -Dpackaging=jar -q
#sudo apt-get install lib32gcc1 libc6-i386
#sudo dpkg -i urtool/*.deb
-
Change to the helloworld example folder and type “mvn install”
-
Copy the target folder or only the “helloworld-1.0-SNAPSHOT.urcap” file to the program folder of the URSim program
-
Load the new URCap
-
It works!
Right now I just use gedit for changing some of the *.java files and play around.
After changing some I type mvn install and create a new *.urcap file.
Thanks for your help so far.
Michael
Thanks, @generalmidi
You can also deploy the URCap directly to the simulated PolyScope by changing the target in the pom.xml
file and run mvn install -Premote ursim
.
The steps to do so, should all be explained in the URCap tutorial.
Hello,
I can now deploy the URCap directly.
I changed the following in the pom.xml file:
The entry ursim.home was empty and now directs to my program folder of URSim.
The entry ursimvm.install.host was empty and now has the value: 10.0.2.15 which is the IP of the virtual machine.
The IP was found by typing “ifconfig” in the console.
This topic was automatically closed 2 days after the last reply. New replies are no longer allowed.